Is Current Limit function available in Altivar 21 Drive
The Current Limit function is available in Altivar 21 Drive. The parameter number is F601.
The Current Limit range is 10-110% of drive's rated current. Factory setting is 110%.
FA86567 |
21-Dec-2012
|
Settings
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is the remote keypad option available for Altivar 21 Drive.
> What does mean "FIRE MODE" in the Altivar drive, in which Altivar model this this function is available.
> What is the difference between Fire Mode (Function 52) and Force Mode (Function 53) in Altivar 21 Drive.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel