What are the Spare Reference Numbers of Finger Contacts and Arms of LF2 (SF6 Breaker).
The spare reference number of Finger Contacts of LF2 (SF6 Breaker) is AAV48765. A single kit contains 6 sets of Finger clusters.
However, the Arm is not available as spare reference, as it requires industrial control jig to verify the perpendicularity during mounting and this is not possible at Site. Moreover it does not get deteriorated in service and thus is not required to be sold as spare part.
Answers which others found helpful |