What are the Auxiliaries that can be used with C60H-DC.
Refer the attached documents for the list of Auxiliaries that can be used with C60H-DC.
1. For the list of Auxiliaries that can be used with C60H-DC as per IEC certification refer attachment 90081.pdf
2. For the list of Auxiliaries that can be used with C60H-DC as per UL certification refer attachment 91103.pdf
Attachment(s):
Answers which others found helpful |