How many Ethernet devices can be connected via ETG100 gateway module at a time.
Total numbers of devices (PLC/HMI) which can be connected on Modbus TCP/IP network to communicate with Modbus slave devices via ETG100 gateway module are as follows:
1 Maximum number of devices for HMI connections: 64
2 Maximum number of PLC devices: 48
Answers which others found helpful |