What is the minimum rating of the Motor that can be used with the Altivar 31/61/71 Range of Drives.
The motor current should not be less than 0.2 times the nominal Drive current when the motor is driven by Altivar 31/61/71 Drives, for thermal protection.
However, the programming of the parameters should be as per the motor nameplate data for safety of the motor.