FAQ Search

What are the different Communication Networks on which the Altivar 61 Drive can be communicated.

The different Communication Networks on which the Altivar 61 Drive be communicated are as follows: 

1. Ethernet TCP/IP
2. Modbus/Unitelway
3. Fipio
4. Modbus Plus
5. DeviceNet
6. Inter Bus
7. CanOpen (In-built)
8. Modbus RTU (In-built)
 
Note:
For communications Point 1 to 6 correct optional communication card needs to be procured.
 
Communication options available for Heating Ventilation and
Air-conditioning (HVAC) System is as follows:
 
1. Lonworks
2. METASYS
3. APOGEE FLN
4. BACnet
 
 
Note:
There is no card available for As-I communication for Altivar 61 Drive.
FA12126  |  21-Dec-2012  | Technical Characteristics
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful