FAQ Search

Does the Energy Reading remain stored for ME range Energy Meters during power failure.

Yes, the Energy Readings remain stored for the ME range meters during power failure as they are stored in the EEPROM.

EEPROM is nonvolatile memory and can store values for a very long time without battery backup.

ME meters are able to keep all the information that has been stored in the EEPROM for more than 10 years. Therefore, a power failure should not pose a problem.

FA12181  |  12-Jul-2012  | Settings
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful