How to establish Ethernet communication between Twido controller and Zelio Logic with Ethernet extension SR3NET01BD.
It is possible to establish Ethernet communication between a Twido controller and Zelio Logic with Ethernet extension SR3NET01BD.
In this communication, user have to remember that Zelio logic relay SR3 series(24VDC Supply)+ Ethernet extension SR3NET01BD will
always act as Slave(Server) on Ethernet network and Twido Controller will be the Master(Client)on Ethernet network).Refer to attached file for
the complete procedure with sample programs.
In this communication, user have to remember that Zelio logic relay SR3 series(24VDC Supply)+ Ethernet extension SR3NET01BD will
always act as Slave(Server) on Ethernet network and Twido Controller will be the Master(Client)on Ethernet network).Refer to attached file for
the complete procedure with sample programs.
Attachment(s):
Answers which others found helpful |