How to connect a 2-Wire sensor to Zelio Logic SR3B261FU.
Refer to attached file for a document illustrating connection of 2-Wire sensor to a Zelio Logic SR3B261FU.
The input impedence to be used is around 350 Kilo Ohms.The resolution illustrate the test in order to avoid
the fact that due to the residual current of the sensor at open state,the Zelio Logic input could be always ON.
the fact that due to the residual current of the sensor at open state,the Zelio Logic input could be always ON.
Attachment(s):
Answers which others found helpful |