Which are the materials used in Compact NSX connection terminals.
The material used in the Compact NSX terminal connectors is as below:
Compact NSX100-250 : Copper (Cu) + Tin coating
Compact NSX 400-630: Copper (Cu) + Silver (Ag) coating
FA22595 |
11-Jul-2012
|
Cabling and Connection
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the material used in Compact NSX connection terminals.
> Is it possible to connect a 3 Pole Compact NSX breaker to use for single phase application.
> Can I connect aluminium or copper, flexible or rigid cables to the single and double terminals of the NSX 400 to 630 range.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel