How to set Clock in the FDM121 Display module of Compact NSX MCCB.
The date and time in the FDM121 display module of Compact NSX can be set either from the supervisor or from the Micrologic software utilities RSU and RCU or from PMC Modbus. It will automatically get synchronized between IFM module, FDM module, BSM module and the Micrologic.
Refer the attachment for the setting details and format of date and time.
Note: If the FDM121 module lost the power like MCCB gets open then the Clock get reset in FDM121 display module. To maintain the clock in FDM121 display module, external supply of 24V DC has to be provided.
Attachment(s):
Answers which others found helpful |