FAQ Search

Is it possible to see the fault current and fault type after tripping in Compact NSX with Micrologic 5 and Micrologic 6.

Yes, it is possible to see the fault current and fault type after tripping in Compact NSX with Micrologic 5 and Micrologic 6. The external 24V DC must be provided to Micrologics. After Fault trip, the type of fault (Ir, Isd, Ii, Ig), the phase concerned and the interrupted current will be displayed by the Micrologic 5 and 6.
FA22603  |  11-Jul-2012  | Settings
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful