FAQ Search

What is the reference of Type A or Type B thermostat in Prisma Plus switchboard.

Type C thermostat is available in Prisma Plus, the part reference of which is 08998. The Type C thermostat Reference 08998 can be used as Type A or Type B by carrying out the modification in the settings and cabling.
 
For making the thermostat Type A or Type B, connect load on the terminal 2 instead of terminal 3 and the supply at L and N. See figures below for details.






FA22631  |  13-Jul-2012
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful