What is the difference between mechanical Interlock EZ2LB0601 & EZ2LB0602 of LC1B Contactor.
EZ2LB0601 comes without bearing & EZ2LB0602 comes with bearing, this is the main difference between these interlocks.
EZ2LB0602 interlock usually is used when the contactor references are the same and can be easily adapted with the contactors.
EZ2LB0601 interlock usually is used with all LC1B model contactors. This interlock allows flexibility to fix the bearing as per the contactor specification to adapt to the mechanical interlock.
Refer the attached sheet for details.
Attachment(s):
Answers which others found helpful |