Is it possible for Magelis XBTGC serial port can be configured for ASCII communication from CoDesys side of SoMachine.
The Magelis XBTGC controller serial port can be configured from the CoDeSys side of SoMachine as follows:
1.Either with SoMachine Network Manager to use SoMachine protocol.
2.Either with Modbus Manager to use Modbus RTU or Modbus ASCII protocol in master or slave mode.
User cannot configure the serial port for use with ASCII Manager.An alternative could be to use Modicon M258 controller
together with a Magelis XBTGT terminal. For M258 Controller,user can configure an ASCII Manager for the serial port.
together with a Magelis XBTGT terminal. For M258 Controller,user can configure an ASCII Manager for the serial port.
Answers which others found helpful |