FAQ Search

Is it possible to get the Earth Fault alarm only without tripping in Compact NSX with Micrologic 6, via Modbus communication.

Yes, only the Earth Fault alarm can be achieved in Compact NSX with Micrologic 6A/6E without tripping the MCCB at Earth Fault.
 
For this, Ground Fault Current (Ig) Settings in Micrologic 6A or 6E has to be set in OFF position and then by using RSU software and SDX module, this feature can be achieved.  
FA22628  |  13-Jul-2012  | Programming
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful