In what type of control station can I install control and signaling units from the Harmony style 5 range?
Harmony style 5 range (XB5) buttons can be used on the front panel of the following control stations:
- XALK, XALD: plastic control stations,
- XAMW: metal elbowed control stations,
- XAPM, XAPJ, XB2SL: metal control stations,
- XAPE: faceplates and empty flush-mounting control stations,
- XAPA: plastic control stations,
- XALG: control stations for severe environments.
- The overall dimensions of all elements including the transformer power supplies for certain indicator lights,
- Stacks of contacts for pushbutton and selector switch type actuators,
- 4-direction joystick controllers,