What are the part numbers of the replacement contact sets for LC1F power contactors?
Spare parts required for each pole of LC1Fxx contactors are as follows:
- 2 fixed contacts
- 1 moving contact
- 2 deflectors
- 1 backplate
- Locking screws and washers
These parts are supplied in complete sets of contacts for each contactor size and are dependant on the number of poles per contactor.
An example of contact set part numbers would be LA5FG431

Part numbers for complete packs of contact sets for LC1F contactors are attached below: