FAQ Search

How many number of maximum devices can be synchronized in CAN Motion bus in LMC058.

 

The Modicon LMC058 Motion Controller is able to synchronize up to 8 devices on CAN motion.
 Do not exceed 8 motion control devices on the CAN motion bus or install any CAN devices. If you do, the CAN motion bus communications may be interrupted, resulting in a loss of synchronization or communication with the controlled devices and unintended operation.
FA134434  |  06-Feb-2012  | Networking
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful