What are the faults that can be reset with the automatic restart function, after the cause has disappeared on Altivar 71 and Altivar 61 drives.
Refer the attached list of the faults which can be reset with the automatic restart function.
Attachment(s):
ATV71_61_Fault.pdf
(PDF,16K)
FA134991 |
21-Dec-2012
|
Technical Documentation
PDF
Email
Bookmark
Print
Answers which others found helpful
> How to switch ACC (Acceleration) & dEC (Deceleration) to AC2 (Acceleration 2) & dE2 (Deceleration 2) in Altivar 71
> What is Obf (Over Braking Fault) in Altivar 71 Drive.
> Is there any possibility to change AFE (Active Front End) DC voltage while it is connected to Altivar 71/61 drive.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel