FAQ Search

Which are the latest GSD file revisions for ProfibusDP communication board of the Altivar 71 Drive.

The latest GSD File revisions required for ProfibusDP communication board of the Altivar 71 Drive are as follows:

 1. The correct revision of GSD File for Profibus Card version V1.1IE01 is revision 3.
 
2. The correct revision of GSD File for Profibus card version V1.1IE03 is revision 5.

Attachment(s):

1.1E01.gsd (GSD,2K)
FA12136  |  11-Jul-2012
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful