What are the Regular, Periodical inspection & Maintenance points for Altivar 71/Altivar 61 drive.
Refer to attached file for
the Regular, Periodical inspection & Maintenance points for Altivar 71/Altivar 61 drive.
Attachment(s):
Inspection and Maintenance_ATV71_ATV61.pdf
(PDF,272K)
FA140831 |
21-Dec-2012
|
Settings
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the Part Reference of Resolver card for Altivar 71 Drive.
> Is it possible to use Altivar 71 Drive for control of the Synchronous Motor.
> Is it possible to connect AFE (Active Front End) with Altivar 71L drive.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel