FAQ Search

What is the time accuracy for Sepam 20, 40, 80 without time synchronization.

Here is some information about the RTC (Real Time Clock) used inside Sepam (whatever the series - 20, 40 or 80):
 
      * The global accuracy of Sepam RTC is 5 ppm at 25°C
      * The used quartz has an accuracy of 20 ppm at 25°C
      * This leads to a global accuracy error of 25 ppm
 
So, the time accuracy drift of a Sepam relay will be equal to 25 ppm * 3600 * 24 = 2.16 seconds per day.
 
Consequently, the drift per year will be about 14 minutes under normal temperature conditions.
FA146675  |  25-Jun-2012  | Technical Characteristics
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful