{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the usage of TSXPACC01 in unitelway communication.

The TSXPACC01 unit is a cabling accessory that connects to the TER connector of the Premium/Atrium PLC processor via
an integral cable fitted with a mini-DIN connector at one end.
This is used to:
  1. Connect several devices to the terminal port of Premium/Atrium PLCs. For this purpose, it is fitted with two mini-DIN                                                                                                       connectors, marked TER and AUX, which are functionally identical to the TER and AUX connectors of the Premium PLC processors.
  2. Isolate Uni-Telway signals in order to extend Premium PLC terminal port links to over 10 meters for the purpose of connecting the PLC to a Uni-Telway bus.
  3. Adapt the bus when the unit is connected to one of the ends of the Uni-Telway bus.
  4. Set the operating mode of the terminal port to Uni-Telway master, Uni-Telway slave or Character Mode
For more information please refer to attachment.

Schneider Electric India

Attachment(s)

TSXPACCC01.pdfTSXPACCC01.pdf [865.78 KB]
Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.