Search FAQs
Does Modicon Quantum comply to IEC61000-4-3 standard
Yes, Modicon Quantum confirms to IEC61000-4-3 standard, IEC61000-4-3 which specify the test method is the "sub-standard" including in IEC61131-2. Schneider has the statement to comply with IEC61131-2.
Inside the official IEC61131-2 document, it mentions the test method confirming to IEC61000-4-3.
Inside the official IEC61131-2 document, it mentions the test method confirming to IEC61000-4-3.
Released for:Schneider Electric India
Explore more
Explore more