What is the KA rating of 29372 and 32623 Busbar Adapters for Compact NS/NSX<630 Circuit Breaker.
The breaking capacity (KA rating) of the system with the Busbar Adapters 29372 and 32623 connected with Compact NS/NSX<630 remains the as the Circuit Breaker connected. By adding the Busbar Adapters only the nominal current of Circuit Breaker is derated (see below table).
| For NS 3P | In | Busbar Adaptor Reference |
| NS100 | 100A | 29372 |
| NS160 | 160A | 29372 |
| NS250 | 250A | 29372 |
| NS400 | 400A | 32623 |
| NS630 | 570A | 32623 |
Answers which others found helpful |