Is TeSys U suitable for DC Motor applications.
All control unit of Tesys U are designed for AC load applications only.
Due to the TeSys U design specifications and accessories limitations, it is not allowed to use Tesys U on DC load.
FA22663 |
21-Dec-2012
|
Hardware Compatibility
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is TeSys U suitable for DC Motor applications.
> Is the Profibus-DP LULC07 communication module compatible with the Tesys U LUTM controller.
> Can the OA1 output of Tesys U be used with multifunction unit to drive a separate motor contactor.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel