Search FAQs
What cable do I need to connect a Zelio Logic smart relay (SR2/SR3) to PC?
The Zelio Logic range of smart, programmable relays have a special communication port which enables them to be programmed and set up using a PC.
The communication ports on a PC are usually USB or 9-way SUBD. Schneider sells cables that are able to adapt to both these types of port.
For the SR2 or SR3 relays:
For the old SR1 range:
The communication ports on a PC are usually USB or 9-way SUBD. Schneider sells cables that are able to adapt to both these types of port.
For the SR2 or SR3 relays:
- SR2USB01: Connecting cable with USB type PC connector, length: 3 m
- SR2CBL01: Connecting cable with 9-way SUB-D type PC connector, length: 3 m
For the old SR1 range:
- SR1CBL01: Connecting cable with 9-way SUB-D type PC connector, length 1.80 m.
- Note that this component is obsolete - this is for information purposes only
Released for:Schneider Electric India
Explore more
Explore more