Search FAQs
Can you use the VW3A1101 keypad with the ATS48 soft starters?
Issue:
VW3A1101 keypad compatibility with the ATS48 soft starters.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Needs to run a 50ft cable run using the VW3A1101 keypad and cat 5 cable to the ATS48 soft starter.
Resolution:
The VW3A1101 keypad is not compatible with the ATS48 soft starter. The correct remote keypad part number for the ATS48 is VW3G48101. The standard cable is 3 meters long. We do not have any test data to support that you can run this cable with a repeater to get a longer cable run out of it. You will have to test to see if the remote cable can mounted longer than 3 meters.
VW3A1101 keypad compatibility with the ATS48 soft starters.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Needs to run a 50ft cable run using the VW3A1101 keypad and cat 5 cable to the ATS48 soft starter.
Resolution:
The VW3A1101 keypad is not compatible with the ATS48 soft starter. The correct remote keypad part number for the ATS48 is VW3G48101. The standard cable is 3 meters long. We do not have any test data to support that you can run this cable with a repeater to get a longer cable run out of it. You will have to test to see if the remote cable can mounted longer than 3 meters.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: