{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is Zelio Soft software compatible with Windows Vista and/or Windows 7, Windows 8 and Windows 10?

Article available in these languages: Dutch

Zelio Soft V5.4.2 is compatible with the following:
  • Windows 7 32bit
  • Windows 7 64bit
  • Windows 8.1 32bit
  • Windows 8.1 64bit
  • Windows 10 32bit
  • Windows 10 64bit
Historic Versions of Zelio Soft
Since Zelio Soft V4.5, it has been compatible with Vista and Windows 7 (W7). However, most installations of Vista and W7 are 64 bit and ZelioSoft V4.5 did not include a 64 bit cable driver, which had to be installed separately (downloadable free of charge from www.se.com/uk)

Note: V4.5 is not compatible with W8.

Zelio Soft V4.6 was released June 2015 , which is compatible with Vista, W7, W8 and now includes the 64 bit driver.

Schneider Electric India

Explore more
Range:
Zelio Logic SR2/SR3Zelio Soft
Explore more
Range:
Zelio Logic SR2/SR3Zelio Soft
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.