Search FAQs
What is the correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket?
The correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:
Please note that the Modbus serial connection function of each pin is as follows :
Pin number 4 (D1): blue wire
Pin number 5 (D0): white-blue wire
Pin number 8 (0 VL): brown wire
Please note that the Modbus serial connection function of each pin is as follows :
Pin number 4 (D1): blue wire
Pin number 5 (D0): white-blue wire
Pin number 8 (0 VL): brown wire
Released for:Schneider Electric India
Explore more
Explore more