Provide sample of Alarm Management in SoHVAC Software for Modicon M168 Controller.
Find attached a sample project which contains the AlarmManagement application function block and a
document which shows the steps to test the project.
document which shows the steps to test the project.
Activate five alarms (2, 3, 4, 7, 98) per default to demonstrate the functionality of the application function block.
If user wants to implement the alarm management in project, user needs to pack the alarm bits to words
(16 Bits to 2 Word in conversion library) and link these words to the input words of alarm management function block.
If user wants to implement the alarm management in project, user needs to pack the alarm bits to words
(16 Bits to 2 Word in conversion library) and link these words to the input words of alarm management function block.
Note that,the application function block does not reset the alarms and it is only for visualization and location of the alarms.
Attachment(s):
Answers which others found helpful |