FAQ Search

How to set RTC(Real Time Clock) in SOHVAC for Modicon M168 Controller.

Using “RTCSetDateTime” function block (with source),user can set the RTC clock of Modicon M168 Controller.Using the said function
block,user can set up the clock using a Modbus register (Double words).
The Date origin is the fist of January 2000.
 
To use this functionality,user can reuse the project or create a Template/Library.Refer to attched document and sample application.

Attachment(s):

FA143331  |  30-Mar-2012  | Settings
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful