Search FAQs
In Ecostruxure Power Design-Ecodial, Is there any limit in connecting number of circuits in the network?
In Ecostruxure Power Design-Ecodial, There is no limit in connecting “number of circuits” on a network.
(But, please consider the maximum rating of the transformer available in Ecodial for the selection. If the network is supplied by a "single" HV/LV transformer, then it can only be loaded up to the available maximum rating of the transformer & it limits the user in connecting number of circuits on the network)
Released for:Schneider Electric India
Explore more
Explore more