{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

With the TSXCUSB485 cable, which Modbus driver should I install for use in Windows Vista Business Edition 32?

The Modbus 2.0 IE10 driver needed for the various Schneider programs which use the Modbus protocol (TwidoSuite, Advantys, PL7) is available in the attachment.
It supports the TSXCUSB485 USB cable and the TSXPCX1031 serial cable.

This attachment is an executable file which includes:
  • The Modbus driver
  • The USB bus Windows driver
  • The virtual serial port Windows driver
Note:
This executable is found in the Schneider V2.6+ drivers pack.

Schneider Electric India

Attachment(s)

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.