FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA170718In a linear load application, is IT earthing acceptable to use AC type C60 Vigi module.
For IT earthing system must use ASi or ASiE devices to avoid nuisance tripping of C60 Vigi modules.   The main reason is due to Neutral line is not...
FA170716Is it necessary to connect the Acti9 range of contactor (iACT24) to the 230VAC power supply.
The 24VDC is just used to send the command, from Acti 9 Smartlink or a PLC. To be able to energize the coil of the associated contactor, the iACT24...
FA170714What is maximum length of the cable between MCB and Acti9 Smartlink.
The cable length between an input of the Acti9 Smartlink and any device connected is limited to 20 meters.
FA170712What's the burden of BCPM power consumption.
 The BCPM is fused at 500mA so, that will be the absolute maximum it could draw, however we expect normal draw to be less than 100mA.   So if the...
FA170617What exactly error E1301 means in Lexium 32 range of servo drives. What precaution need to be taken to overcome it.
 Error E1301 appears if STO (Safe Torque Function) is not triggered via two redundant inputs STO A and STO B simultaneously. It means if STO A and...
FA170616Is it possible to operate or configure ATV303 drive with remote HMI
Yes, it is possible to operate and / or to configure ATV303 drive by means of remote HMI Part reference VW3A1006.
FA170611Does “dIS” on display of lexium servo drive indicates fault. How to overcome it.
“dIS” on display does not indicate fault state of lexium servo drive but it is one of the states of servo drive. dIS stands for Switch ON Disabled....
FA170610When Lexium 32 range of servo drive goes into the “QUICK STOP”.
Lexium 32 range of servo drive goes into the QUICK STOP under two conditions If servo drive meet with an error of class 1 or class 2. Upon...
FA170609In Lexium range drive the permissible range of motor shaft movement if absolute position is to be retained while servo drive is powered off.
Permissible range of motor shaft movement is +/ - 0.25 revolution from the position at which motor shaft position was at the moment servo drive was...
FA170608In Altivar range of drives ,display of current (A) is blinking on 7 –segment LED display. What does this mean.
Blinking of Current (A) displayed on 7-segment LED display indicates that drive has reached to the current limitation. This occurs when current drawn...

Results 1 - 10 of 100