FAQs

FAQ Search
Most Recently Published FAQs

Results 61 - 70 of 100

FAQ ID Description
FA168463How to make factory default the Altivar 312 drive.
In the menu drC [Motor Control]: FCS [Return to factory defaults] :Ini                 Press ENT button on the HMI for 2 seconds until NO appears on...
FA168462How we can run Altivar 312 drive without motor load.
Configure following parameter  FLt (Fault menu) OPL (Output phase loss)= NO.  By setting above parameter, you can check drive without physical connection...
FA168244What is the use of Automatic adaptation of deceleration ramp parameter on Altivar 312 drive.
This function is used to automatically adapt the deceleration ramp if the initial setting is too low for the inertia of the load connected. It avoids...
FA168243What is the meaning of 1:100 speed range in Altivar 71 drive.
Speed range is the ratio of the output maximum frequency/minimum frequency where the nominal torque is available.   Example: For a 50Hz motor   Altivar...
FA168242What is the options of braking resistor for Altivar 71 range.
Refer to attached file forthe part number of braking resistor for Altivar 71 range.
FA168241How to get the Profibus GSD file for Altivar 71/61.
Refer to attached file for profibus GSD file of Altivar 71/61.
FA168240What is the meaning of Err 7 in Altivar 58.
Err 7 is a Time out error, the display has sent a request to the control board and does not receive answer   It indicates a defect of communication...
FA168009Can the GV3 range MPCB be operated by a door interlockable external handle.
Yes, it is possible by using of the GV3AP01 & GV3AP02.
FA168008Is the terminal shield used in Compact NS range MCCb compatible with NSX range of MCCB.
Terminal shields are fully compatible between the Compact NS and Compact NSX ranges.
FA168007Is it possible to connect a 3 Pole Compact NSX breaker to use for single phase application.
If you need to protect a single phase with a NSX in 3P you can connect the load (phase 1) to the pole 1 and the load (neutral) to the pole 3. Pole...

Results 61 - 70 of 100