Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA144505How many PRM modules can Quantum Ethernet NOE module can handle at one time.
The One number of NOE module can handle maximum 7 numbers of PRM modules.
FA136899What version of Unity Pro supports Quantum safety Modules.
Quantum safety modules only supports for Unity Pro 3.1 and 4.1.
FA86516What is the Quantum CPU Firmware & Unity Pro Version compatibility.
One can use any OS/Copro Firmware Quantum Processor with any Unity Version. However it is recommended to use latest OS/Copro Firmware Quantum Processor and...
FA149726Is Concept software is supported on Windows 7.
Yes, Concept Version V2.6 Service Release 7 is compatible with Windows XP Professional, Windows Vista Business 32-Bit and Windows 7 Professional...
FA12116How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range.
140CPU65160 can IO scan up to 128 devices/registers maximum.The total number of input and output words which can be scanned during one cycle is 4000...
FA135503Does TwidoSuite Software support Windows 7 operating system.
The TwidoSuite software V2.20 has not been Qualified with Windows 7 (32 or 64 bits).The TwidoSuite software is qualified for Windows XP,Windows Vista...
FA134935What are the modules in the Quantum range which supports Hart fieldbus.
Quantum modules are able to be connected to Hart fieldbus. Here is the list of our IO Quantum modules with Hart protocol. ACO1300 ACI04000 ...
FA134934Does Quantum Range supports Unitelwy Bus.
Quantum range does not support Unitelwy bus.
FA86475Is it possible that you can EXTEND the Premium CPU Sync Link using fiber cable and fiber Switches.
The use of an optical link with two switches for EXTENDING the Premium CPU Sync Link is forbidden today. Only an electrical copper link with a maximum...
FA27941What replaces the TWD Analog and Discrete I/O modules?
The TWD modules are replaced by TM2 modules as listed in the tables below: TM2 modules are supported by version 2.20 and above of TwidoSuite software....

Results 1 - 10 of 100