Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 83

FAQ ID Description
FA144505How many PRM modules can Quantum Ethernet NOE module can handle at one time.
The One number of NOE module can handle maximum 7 numbers of PRM modules.
FA134935What are the modules in the Quantum range which supports Hart fieldbus.
Quantum modules are able to be connected to Hart fieldbus. Here is the list of our IO Quantum modules with Hart protocol. ACO1300 ACI04000 ...
FA86475Is it possible that you can EXTEND the Premium CPU Sync Link using fiber cable and fiber Switches.
The use of an optical link with two switches for EXTENDING the Premium CPU Sync Link is forbidden today. Only an electrical copper link with a maximum...
FA136529Is it possible to use internal power supply of Twido TWDLCAE40DRF for analogue extension module TM2AMM3HT.
Yes,it is possible to use internal power supply of Twido TWDLCAE40DRF for supplying power to analogue extension module TM2AMM3HT. The compact Twido...
FA144504How many PRM modules can M340 NOE and Premium ETY can handle at one time.
The One number of NOE and ETY module can handle maximum 3 numbers of PRM modules.
FA86515What is the version compatibility for M340 NOE Module (Ethernet) and Processor
The following table shows compatible combinations for M340 NOE Module and M340 Processor: * In this case the NOE module will not be reconized as...
FA134932Are any of the Modicon M340 Analog input modules compatible with HART signals.
M340 Analog modules are not compatible with HART signals.
FA140466What is the maximum number of motion control modules (BMXMSP0200) and/or counter modules (BMXEHC0200, BMXEHC0800) that can be used with a M340 PLC
The maximum number of motion control modules (BMXMSP0200) and/or counter modules (BMXEHC0200, BMXEHC0800) is limited to 36 configured channels, which...
FA12025Where can the embedded Ethernet port of M340 PLC used
The embedded Ethernet port on the M340 processors can be used to connect to the Schneider Electric Magelis range of HMI. For IO scanning NOE module...
FA86681Which are the Encoder Option cards available for Altivar 71 along with their part numbers and specification
Six types of encoder cards are available depending on the Encoder Technology (Incremental or Absolute). 1.) RS 422 compatible differential outputs. 2.)...

Results 1 - 10 of 83