| FA86557 | How to size the Generator or Transformer required for supplying single unit of Drive The size of the Generator/Transformer should be 1.5 to 2 times the power in VA to that of the drive that is to be supplied.
Example: The Power rating... |
| FA86526 | How to connect the Remote Display (HMI) Unit of Altivar 71 via LU9GC3 Modbus splitter The Remote Display (HMI) unit of the Altivar 71/ 61 drive takes it power from the drive port to which it is connected.
When the same Remote Unit... |
| FA86530 | Which Encoder Cards support HTL (High Transistor Logic) signal Encoders for Altivar 71 drive The High Transistor Logic (HTL) is a type of Push Pull. So VW3A3405 or 06 or 07 Encoder option Board, depending on the excitation power required,... |
| FA23075 | Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure? No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure:
1. An SZ1RV1202 potentiometer... |
| FA145819 | Is it possible to use two Extended I/O Cards in one Altivar 71 drive. It is not possible to use two I/O Extension cards in one Altivar 71 drive. However, it is possible to use one VW3A3201 Logic I/O
Card & one VW3A3202... |
| FA134636 | What is the Type1 & Type2 co-ordination chart for Altivar 61 & Altivar 71 with compact NSX motor circuit breaker. Refer to attached file for the Type1 & Type2 co-ordination chart with compact NSX motor circuit breaker selection. |
| FA134983 | Which Altivar Drive model is compatible with Pump card. The Pump card is tested and guaranteed for ATV61 drive only. |
| FA134436 | Is it possible to connect Altivar 312 and Altivar 71 drive on the same DC bus.
The Altivar 312 and Altivar 71 cannot be connected on the same DC bus.
The Over Braking Fault (OBF ) threshold of ATV312 is 880V and the OBF of... |
| FA134445 | Can we use shielded cable with the sinus filter which is used in Altivar 71 and Altivar 61 Drives. It is not recommended to use shield cable when you use sinus filter because the sinus filter and the shield cable generate earth leakage current (due... |
| FA12145 | Is the remote keypad option available for Altivar 21 Drive. Yes, the remote keypad option is available for the Altivar 21 Drive. The reference for the same is VW3A21101. It can be installed remotely up to a... |