Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 41 - 50 of 83

FAQ ID Description
FA12203Can the Multi 9 range MCB be reverse fed.
Yes, the Multi9 miniature circuit breakers (MCBs) can be fed either from top or bottom without any deterioration of their characteristics.   Refer...
FA22772What is the difference between 31088 and 31097 key locking devices.
31097 keylocking device is used for the Single Handle Source Changeover Assembly in which different type off cam is used. These cams are to be ordered...
FA12200What is the maximum rated current for 36KV Fusarc switch.
The maximum rated current for 36KV Fusrac switch is 63 Amps. Refer attachment for the selection of proper fuse.
FA12175Can two Line Chokes be connected in series for Altivar 31/61/71 Drives, in case the correct value Line Choke is not available.
Yes, two smaller Line Chokes can be connected in series for Altivar 31/61/71 Drives.Note:The drop voltage of Line Choke is approximately 3% of the...
FA12124What is the minimum rating of the Motor that can be used with the Altivar 31/61/71 Range of Drives.
The motor current should not be less than 0.2 times the nominal Drive current when the motor is driven by Altivar 31/61/71 Drives, for thermal protection.However,...
FA12080Is it possible to install the Fusarc fuse in the upstream of LBS (Load Break Switch).
Yes, it is possible to install the Fusarc fuses in the upstream of Load Break Switch (LBS) switch. Note: 1. Refer the attached sheet to choose and...
FA12087Provide the maximum length of cable that can be used with Multi9 circuit breakers in TN Network.
Refer attached document for the Maximum length of cable that can be used with Multi9 circuit breakers in TN Network.
FA12183What is the latest Feature and Reference Number of MA500 trip unit for Compact NS630 MCCB.
The new name of the MA500 trip unit is MAE500 or STR13MAE500.The old MA500 trip unit was designed with mechanical feature and new MA trip unit is...
FA12184Is it possible to install OF/SD/SDE Auxiliary Contact (29450) in Single Pole and Two Pole Compact NS MCCBs.
Auxiliary Contact installation is possible in Two Poles MCCBs same as in Three Pole and Four Pole MCCBs, but it is not possible to install and use...
FA12083What is the size of cable that can be used for the remote connection of time delayed UVR/MN module of Masterpact ACBs.
With the increase in length there always occurs a voltage drop in the cable. Refer the attachment for voltage drop values, according to cable sizes...

Results 41 - 50 of 83