Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 61 - 70 of 83

FAQ ID Description
FA22589Can the existing Full Function Test Kit (FFTK) be used for testing the new Compact NSX MCCB.
Compact NSX can be tested with a new dedicated test kit, Maintenance case ref erence TRV00910. This TRV00910 test kit works in association with the...
FA22652Is it possible to change the scaling of Voltage from V (Volt) to MV (Megavolt) on the display of PM820.
The scaling of Voltage at the display of PM820 is changed automatically by the meter as per the Voltage level of the supply.   The PM Meter will change...
FA12106What is the minimum distance required for cable interlocking between two Masterpact ACB’s.
Masterpact Air circuit Breaker (ACB) could be placed just side by side, there is no safety clearance required for cable interlocking between two Masterpact...
FA12105Is it possible to install the rectangular sensor at the incoming side of the Masterpact ACB with Micrologic 7.0.
Yes, it is possible to install the rectangular sensor at the incoming side of the Masterpact Air circuit breaker (ACB).The earth leakage protection...
FA12202How many Mechanical Operations can be done with Evolis Circuit Breaker.
Evolis Circuit breaker comply the Class M2 of IEC 62261-100 Standards. As per class M2 of IEC Standard, the circuit breaker can be operated up to...
FA22602What are the different communication settings available with the Micrologic 5 and 6 in Compact NSX.
There are three types of communication settings achievable as per the hardware used with Micrologic 5 or 6 in Compact NSX.   In config A - With...
FA12103How to deactivate the Earth Fault protection in Micrologic 6.0 trip unit of Masterpact ACB.
To deactivate the Earth Fault protection function in Micrologic 6.0 trip unit, follow the below procedure:1. On the Masterpact Air Circuit Breaker...
FA12102Is it possible to modify the neutral position in Masterpact ACB from left hand side to right hand side.
The offer for Masterpact Air Circuit Breaker (ACB) with neutral position on the both sides is available. This option has to be selected at the time...
FA22779What is the behavior of the EM9 monitoring device if the Neutral & Earth terminals are directly connected.
EM9 Insulation monitoring device (IMD) is used on IT network system. In IT network system Neutral is isolated from Earth. EM9 measure the insulation...
FA12205What are the Shock and Vibration values of C60 range MCBs.
Refer attachment for the Shock and Vibration Values of C60 range MCBs.

Results 61 - 70 of 83