Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 84

FAQ ID Description
FA12205What are the Shock and Vibration values of C60 range MCBs.
Refer attachment for the Shock and Vibration Values of C60 range MCBs.
FA12097How many Ethernet devices can be connected via ETG100 gateway module at a time.
Total numbers of devices (PLC/HMI) which can be connected on Modbus TCP/IP network to communicate with Modbus slave devices via ETG100 gateway module...
FA22591Why is it not possible to have a built in motor mechanism for Compact NS630 LB and NS800 LB Circuit Breakers.
The basic frames of the Compact NS630b LB and NS800 LB Circuit Breakers have been modified as compared to the basic frame for the other Circuit Breakers...
FA144551Is it possible to mount shunt coil ( MX ) and under voltage coil ( MN ) simultaneously in Compact NSX circuit breaker.
In Compact NSX MCCBs either shunt coil ( MX ) or under voltage coil ( MN ) can be mounted in the same slot provided in circuit breaker.
FA136038Is it possible to connect AFE (Active Front End) with Altivar 71L drive.
Regen Connection Parameter is not available for ATV71L drive. So, it is not possible to connect AFE (Active Front End) with Altivar 71L drive. Regen...
FA135006Is it possible to use the braking module VW3A11701 of the Altivar 11 on the Altivar 12 drive.
The braking module VW3A11701 of Altivar 11 can used on the Altivar 12 and vice versa, the braking module VW3A7005 of Altivar 12 can use on Altivar 11.
FA140417Can we mount Compact NS motor mechanism over Compact NSX MCCB.
A Compact NS motor mechanism can only be used on a Compact NS MCCB. However, Compact NSX motor mechanism may be used on a Compact NSX or NS MCCB.  
FA139958Is it possible to install spreaders downstream of the Compact NSX.
Yes, it is possible to install all connection accessories both upstream and downstream of the NSX.  
FA139370Do we have any Type 2 coordination chart for DOL & Star-Delta motor starters operational voltage of 220/240 V AC, 500/525 V AC & 690 V AC.
The Type 2 coordination chart for DOL & Star-Delta motor starters at an operational voltage of 220/240 V AC, 500/525 V AC & 690 V AC is available. Please...
FA138741Can the SDE contact be fitted into a Masterpact NT or NW switch disconnector.
  The SDE contact does not perform any function on a Masterpact switch disconnector and therefore it's not fitted nor is it available as an option.

Results 71 - 80 of 84