Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 100

FAQ ID Description
FA169749Is it possible to use the 3 poles NSX circuit breakers with 3 pole Vigi module on a single phase application.
The Vigi module can be used in a single-phase configuration for a 3P type. The Vigi works in single-phase between two phases, The test push button...
FA169748What is the definition of the term OSN on micrologic electronic trip units.
OSN (Over Size Neutral) means that the neutral protection is 1.6 times greater than the phase protection.   This type of trip unit is used if there...
FA169747How to obtain the manufacturing date code of the Compact NS or NSX circuit-breakers from the MCCB.
To obtain the manufacturing date of Compact NS or NSX circuit-breakers, read the screen-printed marking at the top of the front panel.   For example...
FA168471How can I look at the compilation errors in Vijeo Citect.
When you compile your Vijeo Citect project then a message appears and shows warnings & error messages, if you again want to re-check those messages...
FA168470Where did I find the Citect.ini file in my Windows 7 system.
The citect.ini files in a Windows 7 System will be found in the given below location. C:\ProgramData\Schneider Electric\Vijeo Citect 7.20\Config  
FA168464Does Altivar 212 has options of Ethernet card for communication.
Altivar 212 doesnot have Ethernet card as an option. However you can use ethernet gateways for communication devices on Ethernet protocol.
FA168243What is the meaning of 1:100 speed range in Altivar 71 drive.
Speed range is the ratio of the output maximum frequency/minimum frequency where the nominal torque is available.   Example: For a 50Hz motor   Altivar...
FA168242What is the options of braking resistor for Altivar 71 range.
Refer to attached file forthe part number of braking resistor for Altivar 71 range.
FA168009Can the GV3 range MPCB be operated by a door interlockable external handle.
Yes, it is possible by using of the GV3AP01 & GV3AP02.
FA168008Is the terminal shield used in Compact NS range MCCb compatible with NSX range of MCCB.
Terminal shields are fully compatible between the Compact NS and Compact NSX ranges.

Results 31 - 40 of 100