Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 41 - 50 of 100

FAQ ID Description
FA167851What is the difference between Vijeo Citect Unity Speedlink Dynamic and Unity Speedlink Static.
Vijeo Citect Unity Speedlink Dynamic is a tool used for linking to a Unity Pro *.stu file project file. It makes a dynamic link between Vijeo Citect...
FA167849What is the difference between the “ReportManager” and the “ReportServer” in Vijeo Historian.
Report Manager is a convenient web user interface to the Report Server that enables you to view and administer your reports, data sources, and report resources.Report Server...
FA167822What is the maximum operating temperature & IP of the Remote graphic display terminal of the Altivar 71 Drive.
The maximum operating temperature of the Remote graphic display terminal is 60°C and it has IP 54 Protection.
FA167821What is the benefit of Line Choke for the drive.
Line chokes are used to provide improved protection against over voltages on the line supply and to reduce harmonic distortion of the current produced...
FA167820What is the benefit of Evacuation function on Altivar 71 drive.
This function is suitable for lift application, when there is a power failure; it facilitates the evacuation of people trapped in a lift stuck between...
FA167812Is ION Setup 3.0 software capable of sending an emails.
ION Setup is only intended to configure meters and pull onboard information for certain meters with that functionality. If a customer wants a way...
FA167811Would ME kilowatt hour meter roll back to 0 after reaching maximum display capacity 9999 kWh.
After 9999.99 kWh, the counter will switch to 10.000 MWh. It will continue until it reaches 99999 MWh.   At this point, you must reset your "partial"...
FA167702What is the significance of CPU sync link for Modicon Quantum HSBY processor.
With this link the standby CPU is updated (Program, data transfer from Primary to Standby) after the end of every scan cycle.   The %SW61.6 bit correspond...
FA167188How can I find the license serial number of my Vijeo Citect Key if it`s sticker is not available on the key.
You can simply get your license key number by inserting the key into your system, open Citect Explorer >> Help >> Key Update then it shows like :
FA167187What is the default location of the Project Folder of Vijeo Citect in Windows 7 OS.
By default Vijeo Citect will save it`s project directory in the below given path for Windows 7 OS: C:\ProgramData\Schneider Electric\Vijeo Citect...

Results 41 - 50 of 100