Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 71 - 80 of 100

FAQ ID Description
FA166521Pinout details of Modbus junction box- VW3A8306TF**.
Pinout details of Modbus junction box- VW3A8306TF** is as below,
FA166508Is it mandatory to use heatsink and thermal interface with SSR P range of SSR (Solid State Relays).
SSR P (Panel mounting type SSR) are not with inbuilt heatsink compare to the integrated heat-sink of SSR D (Din rail mounting type SSR) rerlays.   It...
FA166507What is timeout error while communicating with PM1000 & DM6000 meter and what are the reasons for this error.
When a master like EGX, ION Enterprise ,System (PC) sends a query & doesn't receive any response from the Meter  within the wait time then the error...
FA166505For PM1000 meters, when are external CTs and/or PTs required.
External CT is required when the load current to be measured is greater than 6A.   An external PT is required when input voltage greater than 480V
FA166504Can the firmware in a Energy Meter (ELF3200/EM6400/PM1200/DM6200) be upgraded.
The firmware in any Conzerv Meter (ELF3200/EM6400) or Schneider-branded Conzerv Meter (DM6200/PM1200) cannot be upgraded.
FA166503Do I need DISABLE the File and Printer sharing option of my PC to get ION Enterprise Web Reporter to work.
The File and Printer Sharing option must be disabled in ION Enterprise systems installed on OS . This must be done during the install of ION Enterprise V...
FA166502What is the maximum number of registers the Modbus Device Importer (MDI) can configure and support.
Maximum is 255 registers per module. 4095 modules per manager. 128 managers.
FA166501Can the VLT Ref 16060 (analogue voltmeter) be used on DC voltages.
 VLT ref 16060 is usable for AC voltages only within the range of 50-60 Hz. You cannot use it on DC voltages.
FA166499What are the factory default settings in DM6000 series.
The factory default settings in DM6000 series is as below, SET Parameter ...
FA166497Is it possible to use the reference LA9D901 with the reference LADR, LADS2 etc.
The LADS2, LADR* and LADT* are time delay auxiliary contact blocks. Each reference respond to distinct need, however theirs external design are identically.   Hence,...

Results 71 - 80 of 100