Narrow By
  1. Your SelectionAll

Technical Characteristics - FAQs

FAQ Search
Most Recently Published FAQs

Results 91 - 100 of 100

FAQ ID Description
FA166407How to upgrade the firmware for BMXNOM0200 module.
Make sure the CPU is in stop mode and the power supply while up gradation should not go off. Use Unity loader Software V2.2 and above to upgrade...
FA166404How to identify the Firmware version of EM6400/DM6200/PM1200.
There are 2 different methods to determine the firmware level in EM6400/DM6200/PM1200 meter if there is no  communications with the meter 1-The label...
FA166400How many PID function blocks can be used in ATV-IMC controller.
As such there is no fix figure exists regarding nos. of PID control Function blocks to be used in application. The limitation will come from memory...
FA166399Which range of ATS22 soft-starter suitable for inside motor winding delta type connection.
ATS22***Q range can only be used with Inside Delta type of connection from range ATS22. So, be ensuring that ATS22***Q has been selected.  
FA166396When bypass contactor switch over takes place in Altistart 22 soft-starter.
When Altistart 22 starter is started, current increases and reaches to a particular peak value depending on load and then starts decreasing. When...
FA166395Give zelio smart relay SR1 to zelio smart relay SR2 correspondence table while transferring zelio-soft V1.5 program running on zelio smart relay SR1 to Zelio smart relay SR2 using zelio-soft V2.0.
While transferring zelio-soft V1.5 application to zelio-soft V2.0 application to make program of zelio smart relay SR1 compatible to run on zelio...
FA166394How to make zelio smart relay SR1 applications (*.zel) compatible to zelio smart relay SR2 / SR3 (*.zm2)
 Zelio softV2.0 is available to convert program of Zelio smart relay SR1 range to Zelio smart relay SR2 / SR3 range provided the application program...
FA166392How relay output and solid state output differs from each other.
Solid state outputs are entirely electronic and involve no moving parts and so service life is increased.   Relay outputs which are most common type...
FA166391Where I can give user`s privilege in Vijeo Citect V7.20.
You can set the user`s privilege in Vijeo Citect Project Editor >> System >> Under “Roles” Configuration. You can use this Roles further in USER...
FA166390Can I connect a client with Vijeo Citect Lite IO Server.
No with Vijeo Citect Lite license you can only run the Vijeo Citect Server in standalone mode only as networking is not allowed in VJC lite license.

Results 91 - 100 of 100