FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA243359What is the Insulation voltage (Ui) of STI isolatable fuse-carriers.
The Insulation voltage (Ui) of STI isolatable fuse-carriers is 800V.
FA243361What is the Degree of protection of STI isolatable fuse-carriers.
The Degree of protection of STI isolatable fuse-carriers device in modular enclosure is IP40.
FA243360What is the Pollution degree of STI isolatable fuse-carriers.
The Pollution degree of STI isolatable fuse-carriers is 3.
FA243367What is the maximum dissipated power per pole of STI isolatable fuse-carriers.
The maximum dissipated power per pole of STI isolatable fuse-carriers is given below:  
FA243364What is the Operating temperature of STI isolatable fuse-carriers.
The Operating temperature of STI isolatable fuse-carriers is -20°C to +60°C.
FA243368What is the storage temperature of STI isolatable fuse-carriers.
The storage temperature of STI isolatable fuse-carriers is -40°C to +80°C.
FA243435Is SoMachine supported on Windows 8.1 operating system.
Yes, SoMachine V4.1 Service Pack1 is supported on following operating system: 1. Windows 7 32bit/ 64 bit 2. Windows 8.1 32bit/ 64 bit
FA243434How can we cold reset LMC078 from application in runtime without doing power cycle.
To reset the LMC078 controller on Cold Restart from application by trigerring any input or event, you can use function block FC_SysReset.
FA243424Is EXCH instruction still available in-spite of communication function blocks (READ_VAR and WRITE_VAR) in SoMachine Basic.
Yes EXCH instruction is still available. The READ_VAR and WRITE_VAR is implemented just to provide easy user program interface. You can use both...
FA243423When EWF (Enhanced Write Filter) is enable in iPC loaded with embedded operating system (Magelis Smart HMIPSC7**** and HMIGTW7353 operating system) we cannot make any permanent changes in iPC. Is there a way to exclude some file or folder from EWF.
The Enhanced Write Filter (EWF) Manager minimizes the number of write operations to help extend the life of the CF Card. It loads temporary data (for example,...

Results 1 - 10 of 100