FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA228005What are the consituents of TeSys LE1M35*** non-reversing D.O.L starters.
The standard version of TeSys LE1M35*** non-reversing D.O.L  comprises: > 1 TeSys contactor LC1 K**, > 1 TeSys thermal overload relay LR2 K, > 1...
FA241384Why PM810 Min/Max value reset on auxillary control power recycle.
There could be the reason that the PM810 without log module, does not have a BIOS battery.   Because, PM810 is without datalog module if control power...
FA241383How to upgrade a ECC or EGX firmware via the command line
To upgrade a EGX or ECC firmware via the command prompt: 1. Open the command prompt (Start > run > type cmd and hit enter). 2. Type FTP and hit enter 3....
FA241382What do the Modbus error codes for the EGX300 mean?
Below is a list of the Modbus error codes for the EGX300. Error Code Modbus Error Description 0x8072 MODBUS...
FA241381How to set SNMP parameters on an EGX100 or EGX300 to view the networking status and diagnostics the gateway
EGX100 and EGX300 support SNMP protocol only on allowing a network administrator to remotely access an EGX with an SNMP manager (SNMP Server), and...
FA241380How to configure the EGX with the information obtained from network administrator.
Before configuring the EGX, obtain a unique static IP address, subnet mask, and default gateway address from your network administrator. Use a Web...
FA240987How position accuracy can be increased on SD326 stepper drive
Stepper drives SD326 includes Switch S1.1 to S1.3 use to set nos. of steps . Switch S1 having 1st three  3 dIP switches namely S1.1, S1.2 & S1.3 Find...
FA240986What is the option, if no movement is desired from BRS3** stepper motor in the event stepper drive SD326 / SD328 is in fault state or powered OFF
In the event of fault, stepper drive's power stage would be disabled immediately and no current would be supplied to the motor. Stepper drive SD326D***...
FA240975Is it possible to use Altivar 71 drive with synchronous motor and encoder feedback signal of type SinCos 1 Vpp
Yes, it is possible to provide speed feddback of signal SinCos 1 Vpp to ATV71 drive. For this user must use ATV71H***N4383 drive(V1.7 and higher)...
FA240974Is it possible to save Homing Method to Stepper drives SD328 range. If yes, how to save.
For Stepper driver range SD328, firmware version V1.501 or higher include parameter “SaveHomeMethod” that allows to save preferred homing method....

Results 1 - 10 of 100