| FA170509 | Where is the Test Button resistor connected between the poles of Vigi iC60 devices (3P and 4P). The Test Button resistor is connected between the poles 2 and 3 of Vigi iC60 devices (3P and 4P).
Please refer the below diagram
|
| FA170508 | What is the earth fault loop impedance values (Zs) for the Acti9 iC60 MCB’s. The earth fault loop impedance values for Acti9 iC60 are given in below table.
|
| FA170507 | How many stop bits does the EGX support.
All EGX devices use an 11-bit frame serial frame. 1 start-bit, 8 data-bits, and 1 or 2 stop bits
depending on the parity selection.
Even parity:... |
| FA170506 | Is it possible to enable "Auto Scrolling" for the EM6400 series meter display. Auto Scroll allows the user to monitor a group of Display Pages sequentially, every 5 seconds, without constant key pressing.
There are three different... |
| FA170505 | Is there any difference in CT wiring of PM800 and PM200/PM700 for Three-Phase 3-wire Power Systems when using 2 CTs. For 3-wire, three-phase systems with 2 CTs, its required to connect terminal S2 = X2 of CT1 to the I2+ terminal of
the PM200/PM700 instead of the... |
| FA22590 | What is the selection criterion of Circuit Breakers for the Capacitor bank application. The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase... |
| FA170013 | After running for a few seconds, Data Service will automatically stop without any prompts. Backfill can cause the symptom. If "ToTime" attribute is earlier than "FromTime" attribute in a backfill record. Data service will consider it as... |
| FA170012 | What is difference between floating point and static point licensing in Vijeo Citect. A client license can be static or floating depending on requirements
Static client license: For operators needing access to the system at all times,... |
| FA170011 | How to exit the vijeo citect from demo mode. When you start Vijeo Citect runtime it will check for the license key and if did not found any valid license then
automatically starts in demo mode.... |
| FA170008 | How do I use Microsoft Windows Media Player ActiveX in Citect. You will need to set the Media Player ActiveX object property to specify the filename that needs be opened and also call the Play Method via Cicode:
1.... |